A world-first – LED Strips with IO-Link Controller from item Industrietechnik

Indicator lights and machine traffic lights have become a firmly established aspect of intralogistics operations, providing information about operating statuses and fill levels. In most cases, however, companies are restricted to...

Further Infos

Handball-INKLUSIV: item unterstützt Sportprogramm von Max-Camp e.V.

Die item Industrietechnik GmbH fördert ganzjährig gemeinnützige Organisationen, die zum gemeinschaftlichen Leben in und um Solingen beitragen. Mit einer Spende von 1000 Euro unterstützt das Unternehmen den max-camp e.V, der sich für...

Further Infos

Using lean production to significantly improve processes

Combining short delivery times with efficient, flexible manufacturing, lean production has been regarded as standard practice for cutting-edge manufacturing ever since the 2000s. Numerous lean methods are available to help companies...

Further Infos

A cobot for any application – how the “INNA” robot cell supports SMEs in production

The skills shortage is driving the development of collaborative robots (cobots), which are now even taking on complex joining processes such as welding. DAST Schweisstechnik GmbH, for example, has decided to use the “INNA” robot...

Further Infos

item showcases new intralogistics solutions

Intralogistics is all about moving materials quickly, which is where the new solutions from item come in. At LogiMAT 2024, the pioneer in building kit systems for industrial applications is exhibiting an ingenious innovation for...

Further Infos

Railing system – safe guidance for individual and bulk goods

Whether goods are large or small, wide or narrow – the item railing system 8 D8 guides all kinds of materials, accommodating loads of up to 250 N, on conveyor belts designed for this purpose. The system, which can easily be adapted...

Further Infos
Katja Feldmann
Press contactKatja FeldmannFriedenstraße 107 - 109
item Industietechnik GmbH
D - 42699 Solingen
+49 212 6580 5427[email protected]
Jan Leins
Press contactJan Leinsadditiv.
Herzog-Adolf-Straße 3
56410 Montabaur
+49 2602 95099-16[email protected]
en
Language
Country
Germany
Find global partners