Select a category All (120) Machine cabins (19) Industrial work benches (19) Protective enclosures (4) Linear System (14) Platforms & stairways (4) Trolleys (6) Racks (5) Lean Production (8) Hygiene protection (9) Robotics (19) Clean production (6) Ergonomic D30 rack Art. no. EX-01094 This mobile rack has two inclined removal slopes that function as feed-in levels and are positioned at optimum reaching height. The lower portion is used as a return line.... Read more Material provisioning rack on castors Art. no. EX-01051 The added boost for efficient production logistics. This material provisioning rack from item comprises three inclined provisioning levels that are loaded according to the... Read more Ergonomic material handling with hand-operated Karakuri/LCA mechanics Art. no. EX-01126 The magazine-based supply solution uses low-cost automation to make light work of restocking work benches. Pulling the lever automatically triggers two functions: The current... Read more Complete 5S cleaning unit with Drawbars for connecting to a tugger train Art. no. EX-01125 Keeping the production area organised: Utensils such as a dustpan and brushes can be securely fitted to the cleaning trolley thanks to the many hooks. Two Waste Bins, plenty... Read more Lightweight and compact cleaning trolley with 5S features Art. no. EX-01117 This CIP cleaning trolley has cleaning utensils such as a brushes and a dustpan fixed in place on one side with the hook and holder system. The front side features storage... Read more Mobile standing desk with complete computer workstation Art. no. EX-01067 This incoming goods trolley has been designed as a work bench for a computer, where sufficient space is also required for writing by hand. The writing surface is arranged... Read more Practical hand trolley with working surface and storage levels Art. no. EX-01035 This transport trolley provides the flexibility that variable production systems demand – in full accordance with Kanban principles. The basic frame can be assembled and... Read more Shelf for intermediate store with roller conveyors Art. no. EX-01035 Everything is light. Lightweight, cylindrical profiles provide a stable, light frame. And the innovative Line D30 from item makes light work of assembly. The only tool needed... Read more