item is now extending its tried-and-tested automation portfolio to include an integrated all-in-one system made up of Linear Units, drive elements, Motors and Controllers. The new item linear motion units® will be unveiled to the public for the very first time at SPS IPC Drives.
Through this new technology, which is simple, reliable and fast, item is creating a platform that will enable companies to harness the potential of digitalisation for linear technology in an Industry 4.0 concept. With the aid of software, customers will be able to select and commission Linear Units, drive elements, Motors and Controllers to suit their applications. This approach will help deliver a quantum leap in the design and dimensioning of automation technology.
Straightforward design and outstanding practicality
It’s what is inside that counts – and that is the principle that Solingen-based company item followed when designing its Line XMS. This line features an ingenious design that is extremely practical and thus perfect for modular series production. For example, XMS can be used to create custom machine enclosures that are optimally geared toward the relevant area of application. The frame design is deformation free and thus exceptionally strong.
Depending on the application scenario, the individual functional sections can be separated to maintain a clear distinction between process, service and supply levels. The door concept is also unique on the market and gives users the opportunity to install custom doors, so that the individual functional areas can be accessed separately, for example. This makes it far easier to carry out maintenance and service work on the machinery.
Another highlight of Line XMS is the cable conduits that are integrated into the profiles and thus ensure that cables and lines can be safely routed to where they are needed. A special Partition Profile can be used to keep power and control cables apart. What’s more, the outer surfaces and seals of the profiles are also smooth and unbroken. The end result is that users benefit from cleaner production operations and effective noise insulation. The line has won multiple design awards.