item is expanding its portfolio of door solutions with its new double doors. Aluminium profiles up to 6,000 mm long enable large, sealed passageways – for example, for transporting bulky structures or wide goods. Thanks to coordinated components, the two door leaves are easy to construct, can be customised and lock reliably.
Whether in clean rooms, machine cabins or production facilities – large passageways are often required that must also be securely closed. With the new double-leaf doors, item now offers a solution that is precisely tailored to these requirements. The design is based on the proven item modular system and enables passageways in customised dimensions.
Secure locking for flexible door solutions
The new fixed leaf complements the familiar Passage Door 8. Depending on requirements, either one leaf or both leaves of the door can be opened. The new, narrow Door Profile 8 80x40 forms the inside of the fixed leaf and also serves as a stop for the active leaf. The new, internally running Edge Bolt 40 ensures that the fixed leaf is reliably locked. When closing, one round bar is pushed down into the floor recess and the other up into the strike plate in the door frame. A circumferential seal ensures that the doors close securely and tightly, even in sensitive areas such as clean rooms. Additional elements such as the door profile cover cap set 8 protect the cut edges.
With the new double-leaf door, item offers users greater freedom in designing functional and secure door solutions. Individual doors can be put together in just a few steps in the item Online Shop, and the configurable assemblies can be customised with millimetre precision. The rule-based online software takes care of all the details.
Further information is available in the e-paper: Neuheiten-2025.pdf
Status: 19 November 2025
Length: 2,114 characters including spaces
Image data: 3 (© item)
Captions
Image 1 The new double doors from item can be used to equip clean rooms or cabins with large passageways.
Image 2 The new internal edge bolt ensures that the fixed sash is securely locked.
Image 3 The narrow 8 80x40 door profile forms the inside of the fixed leaf.